Climate control, energy recovery and clean technology solutions
While perhaps best known for its dehumidification solutions, Munters also provides a range of climate control, energy recovery and clean technology solutions for critical commercial and industrial production processes.
Applications for general industry
Prevent corrosion, mold and mildew
Keeping the indoor relative humidity at a low level prevents the formation of condensation, which can cause corrosion, mold and mildew. Heating the air to maintain appropriate relative humidity levels consumes unnecessary energy. Munters desiccant dehumidifiers remove moisture and maintain optimal relative humidity levels without increasing the temperature, thereby delivering substantial energy savings in industrial applications.
Contact Munters to inquire about our wide range of climate control solutions for all types of production.
Advantages:
- Prevents mold, mildew and corrosion
- Protects electrical systems
- Reduces energy costs without increasing the temperature
- Lowers maintenance costs
- Provides a more comfortable work environment
Better air quality and working environments
Indoor air quality (IAQ) is compromised by pollutants, such as dust, pollen, mold, mildew and volatile organic compounds (VOCs). Long-term exposure to poor IAQ can contribute to chronic respiratory illnesses such as asthma.
Increasing ventilation in buildings without compromising indoor humidity is challenging. Munters uses two time-proven technologies: energy recovery to eliminate waste and desiccant dehumidification to ensure relative humidity levels fall within an acceptable range that meets ASHRAE standards for building comfort. In addition, Munters provides Zeolite rotor concentrator systems, which are both cost- and energy-efficient. These remove VOCs from the air while improving the working environment and the environment as a whole.
Contact Munters to inquire about our wide range of climate control solutions for all types of production.
Advantages:
- Better indoor air quality
- Increased comfort levels
- Reduced operating costs
- Compliance with ASHRAE guidelines
Perfect storage conditions
One of the main concerns of the owners of warehouses and storage facilities, especially those containing sensitive or delicate goods, is excessive moisture. It can result in costly and disruptive damage to many commonly stored goods, such as metals, powder, food, electronics and clothing, not to mention the equipment in the storage facility itself.
While improving the insulation of the building will ease the problem, a long-term solution is required to maintain the perfect climate. Installing Munters dehumidification devices moves moisture-laden air outside or condenses the moisture into water, keeping stored goods in optimal condition.
Contact Munters to inquire about our wide range of climate control solutions for all types of production.
Advantages:
- Protect stored goods and equipment
- Prevent mold, bacteria and corrosion
- Control indoor climate year-round
- Ensure a comfortable climate for building occupants
- Reduce energy costs
Combined temperature and humidity control
Manufacturers must often control temperature and humidity independently. Munters energy-efficient industrial air conditioning systems make smart use of desiccant rotor technology to handle various combinations of temperature and humidity control.
Munters optimized industrial humidity removal and dedicated outdoor air systems (DOAS) are capable of delivering very dry air to manage peak latent design conditions in controlled spaces. Additionally, they can operate at reduced input capacity to minimize energy consumption and offer more moderate humidity levels of supply air during periods when the controlled space's latent load is less severe. The systems maintain the desired temperature and humidity conditions for the space while offering exceptional flexibility to respond to wide fluctuations in temperature and humidity in an energy-efficient manner.
Contact Munters to inquire about our wide range of climate control solutions for all kinds of production.
Advantages:
- Precise climate control, as needed
- Maximum flexibility
- Reduced energy costs
Energy-efficient solutions for cleaner process
Clean technologies solutions from Munters features mist elimination and gas-liquid separation systems to help wherever liquids and gases require separation, mass transfer technology to separate chemical components and facilitate liquid extraction and VOC abatement to remove pollutants from the air. Clean technologies enhance process productivity while reducing emissions.
Contact Munters to inquire about our clean technology solutions for all types of production.
Advantages:
- Leading industry expertise
- Improve production and energy efficiency
- Lower emissions
- Reduce your carbon footprint
Energy-efficient cooling
Munters is a global leader in evaporative cooling solutions. Our direct and indirect evaporative cooling technologies are sustainable and energy efficient, using nature’s own way of cooling.
Munters evaporative cooling solutions include direct evaporative coolers, where liquid water is transformed into vapor and released into the air using an engineered pad to provide adiabatic cooling, and indirect evaporative coolers, where evaporating water cools the scavenger air as it passes through a heat exchanger, thereby maintaining constant humidity in the conditioned space. Direct and indirect evaporative cooling technologies are extremely energy efficient, negating the need for compressors in the cooling cycle.
Contact Munters to inquire about our cooling solutions for all kinds of production.
Advantages:
- Leading industry expertise
- Sustainable and energy efficient
- Reliable and cost-effective
- Available for a wide range of cooling needs