Munters AB has divested its FoodTech Equipment offering to Grain & Protein Technologies, owned by American Industrial Partners. As a result, neither Munters AB nor any of the companies within the Munters Group are responsible or liable for any content related to FoodTech Equipment that temporarily remain on the website or for any products or services related to FoodTech Equipment, except to the extent required by applicable law. This includes any inaccuracies, errors, or omissions in the information provided. For more information, please refer to the press release dated 9 February 2025, available at https://www.munters.com/en-us/news-media/press-releases/2025/munters-signs-an-agreement-to-divest-the-foodtech-equipment-offering/.
Greenhouse cooling techniques

Temperature control is paramount for greenhouse cultivation. Uncover effective cooling techniques that help your plants beat the heat and thrive, even in scorching outdoor air conditions.

Forced ventilation with evaporative cooling
Ventilation and evaporative cooling can be used together to create a very efficient cooling system for greenhouses. The ventilation system can be used to remove hot, humid air from the greenhouse, while the evaporative cooling system can be used to cool the incoming air. A fan-powered ventilation system, for example, can remove hot, humid greenhouse air through a series of vents. An evaporative cooling system can then lower supply air temperature by passing outdoor air over water-saturated pads.
By using ventilation and evaporative cooling together, growers can create a comfortable and productive environment for their plants, even in hot, humid climates.

Pad and fan cooling techniques for greenhouses
Munters CELdek® evaporative cooling pads are ideal for greenhouses that require high-efficiency cooling. The unique cross-fluted design directs more water to the air entering the pad, where the most intense evaporation occurs. The result? Cooler, more humid air that can help to improve crop yields and reduce energy costs.
Incredibly durable, CELdek pads resist deterioration due to unique, chemically treated cellulose paper. The pads withstand repeated cleaning and severe weather conditions, extending their service life.

Automated cooling with Munters Green Climate Controller
Effectively cool your greenhouse while improving your yields with Munters Green Climate Controller. This comprehensive climate control system creates a cool and comfortable environment for your plants, even on the hottest days.
Its automated control system can automatically adjust the ventilation, shading and misting systems in your greenhouse to maintain a consistent temperature and humidity level. Take the guesswork out of greenhouse climate control and save time and effort to regulate your indoor climate.
Explore digital greenhouse control with Munters Green Climate Controller

Balancing cooling and humidity in your greenhouses
While cooling systems effectively reduce temperatures, they can inadvertently elevate humidity levels, creating an environment ripe for fungal growth. Achieving the delicate balance between cooling and humidity control requires finesse and expertise.
An intelligent climate control system like the Munters Green Climate Controller lets you regulate temperature with precision and fine-tune humidity levels, creating an optimal environment for plant growth. Moreover, during periods of elevated humidity outdoors, your climate control system can automatically adjust the cooling mechanisms to prevent excessive moisture buildup inside the greenhouse.

Controlled cooling in an enclosed environment
Efficient cooling in an enclosed greenhouse offers benefits such as:
-
More effective cooling: Evaporative cooling can be more effective at reducing greenhouse temperatures than natural ventilation, especially in hot and dry climates. This is because evaporative cooling can cool the air to a lower temperature than natural ventilation.
-
Improved plant growth: Evaporative cooling can help improve plant growth, providing the humidity plants need to thrive. This is especially important in hot, dry climates.
-
Reduced risk of disease: Evaporative cooling can help reduce the risk of plant disease by removing hot, stale air from the greenhouse. This is because disease is more likely to spread in warm, humid environments.
-
Energy savings: Evaporative cooling is a relatively energy-efficient way to cool greenhouses. It uses only a small amount of electricity to pump water through the cooling pads and does not require any additional refrigeration equipment.
Investing in effective cooling isn’t only about comfort; it’s about maximizing productivity in your greenhouse.