Munters’ rental service in Japan attracts big customers

May 25, 2022

During the summer months, many companies in Japan struggle with moisture and the result this has on their business.

Our rental solutions are used by many large companies for a wide variety of applications, including rust protection, sandblasting and condensation control.

The service gives customers the possibility to rent energy-efficient dehumidifiers and air treatment solutions on a flexible short-term basis, as long as they need them, without the long-term commitment.

An example of its use is when an art gallery rented a dehumidifier to stop copy paper from jamming when the humidity reached more than 80%. Other companies have used our rental service to prevent corrosion of conveyor belts or to combat condensation in refrigerators.

"It's great to see that there is an interest in our rental service,” says Paul Roberts, Director of Services for APAC at Munters. “It gives customers a chance to test our equipment without committing to buying from us and helps them solve the issue of humidity flexibly.”

Our rental service is available worldwide. For more information, click here.