Evaporative humidification and cooling

Get the optimal indoor climate
Munters evaporative (adiabatic) humidification and cooling solutions help maintain indoor environments in industrial, office and commercial buildings. Maintaining the correct relative humidity levels to prevent static electricity and dust-related problems ensures the well-being of building occupants. Using an evaporative humidification and cooling system improves temperature and relative humidity control and reduces energy consumption.
Munters solutions:
- Increase production quality and minimize production rejects
- Create a healthier indoor climate
- Obtain precise temperature and relative humidity
- Lower operating costs in some applications
The sustainable way to optimal humidity
Munters is a global leader in developing and manufacturing energy-efficient evaporative humidification solutions. Our hygienic climate control solutions are powered by sustainable energy sources. Munters evaporative humidifiers and coolers speed up the process of natural evaporation to create indoor environments that are healthy, productive and sustainable.

How does it work?
Evaporative humidification and cooling systems use a process that adds water molecules to the air, increasing the relative humidity and lowering the temperature. Depending on your specific application, the desired objectives can include achieving higher humidity levels or reducing the temperature.
Certified safety

Legionella
Legionella is a group of bacteria that thrives in aquatic environments. They can also be present in industrial environments such as cooling towers, evaporative condensers, and other water-based systems. If not properly controlled, Legionella can rapidly multiply and become airborne. Inhalation of Legionella-contaminated aerosols poses a significant risk to human health, potentially leading to Legionnaires' disease. Currently, there are 52 identified species of Legionella.
Read more

GREENGUARD Gold certification
Did you know that people spend over 90% of their time indoors? It might surprise you to learn that the primary source of indoor air pollution stems from chemical emissions released by building materials and furnishings. That's why Munters is proud to offer CELdek® and GLASdek® evaporative cooling and humidification pads, both of which have earned GREENGUARD Gold Certification from the independent UL organization.
Read more

Calculate your cooling profit
Compare Munters GLASdek GX40 high-performance evaporative media against any other industry standard brand to see how investment and costs carry out yearly as well as during a 10 year period.

Year-round climate control needed
As the seasons change, so do the humidity levels, outdoors and in, since treated indoor air originates outdoors. Humidity levels inside drop in the winter, leading to dry skin, itchy eyes, and throat irritation if the proper levels aren’t maintained. If not treated, moisture-laden summer air can cause bacteria and mold, spreading airborne microbes and pollutants throughout buildings.
Product overview
Discover our series of energy-efficient evaporative humidifiers designed for all climates, indoor spaces and applications. Suitable for all requirements, we can customize solutions to suit your specific needs.